Other Parts Discussed in Thread: OPA657, OPA846, OPA847, OPA656, THS4520, TINA-TI, THS3202
Hi everybody,
I'm roughly a newbie in analog electronic design. So, forgive me if the question appear to be a bit stupid.
Actually, I'm a physicist and I try to design a transimpedence amplifier for high gain and low capacitance ( 1pF) Avalanche photodiode.
I need an intermediate circuitry to be connected to an already available (50 ohms input impedence) ADC module. The ADC range is 4 V.
The expected current range from the APD (bias : 50 V) is 10fC - 2 pC , pulse width 20 ns. I need only a limited transimpedence gain of 1000 but the noise has to be really reduce to the lowest possible value. Of course, high bandwith is necessary. reasonable linearity is also needed all over the charge range.
The best would be to get differential ouputs. However, this is not mandatory.
I intent to use the OPA 657 amplifier, APD AC coupled to the inverting input, with a 1 kOhm feedback resistor and no feedback capacitance as a first stage. Is it reasonable ?
Would you, guys, have any better idea ?