1. I am trying to choose the op-amp, op-amp application is
a. Input for the op-amp is from frequency to voltage converter - LM2917
b. Power supply for op-amp is 0V & 12V
c. Op-Amp Input voltage range : 0.4V to 8V
d. Op-Amp is configured as Non-Inverting amplifier with gain of 2 (1+1K/1K)
e. Op-Amp is going to drive fuel gauge - 0.03 A to 0.400 A
2. Initiall I tried with OPA-547, but the constraint is minimum output is 1.6V so dial on fuel gauge drastically falls from 1/2 indicator or Empty indicator.
3. Can you suggest me an op-amp? I tried in the posts, but didn't find any nearby answers, if there are any posts then let me know, i will look into the suggestions.
Other question is :
4. If I want to go with opa 547, then I is to provide -2V instead of 0V, what should be the soruce current is it+/- 10mA?
5. Are there any +12V to -2V or -5V converter that can support opa 547
Thanks