Other Parts Discussed in Thread: LM311, LM311-N
I've been evaluating the LM311 Comparator for 1mV to 10mV input signal changes and have been attempting Figure 40 in the Data Sheet. I've been following the Application Hints - but I expect maybe not as well as some need to be done.
I am getting oscillation as the output ATTEMPTS to change state. I say ATTEMPT as I can hold it right at the point where it goes into oscillation, without the hysteresis pulling it through.
I've read the application notes and have now tried three prototypes.
In the book, Trouble Shooting Analogue Circuits, Bob Pease mentioned LM311 troubles (in the chapter described below).
Obviously many engineers have experienced trouble here before.
The chapter text suggests that Bob Pease had solved the problem and possibly documented a solution. I can't find this on the web. Possibly it is help within National Semiconductors archives.
Does anybody know if anything exists? It may even be within one of his many paper-pad hand-drawing style articles.
Straight searches find heaps of LM311 hits, but nothing on Bob Pease's solution.
-----------------------------------------------
Chapter 9. Quashing Spurious Oscillations
Page: 113 1st new paragraph.
Just the Right Touch
For faster comparators, such as the LM311, everything gets even touchier, and the layout is more critical.
Yet, when several people accused the LM311 of being inherently oscillatory, I showed them that with a good layout, the LM311 is capable of amplifying any small signal, including its own input noise, without oscillating and without any requirement for positive feedback.
-----------------------