Other Parts Discussed in Thread: PGA280
Hello
My customer has following issue:
They observe signal distortion above 20kHz when they set the PGA280 gain to 1/8. See attached file.
Is this behavior normal case? or what could be the cause for it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PGA280
Hello
My customer has following issue:
They observe signal distortion above 20kHz when they set the PGA280 gain to 1/8. See attached file.
Is this behavior normal case? or what could be the cause for it?
I got this response from the designer:
***
Yes, we have seen distortion at large signals with increasing frequency. This is at a little bit lower frequencies than what we have seen, but still in the ballpark. It has to do with the general architecture of the part. As the topology strongly relies on current conservation for accuracy at higher frequencies parasitic capacitances lead to loss of current that show up as distortion on the signal.
***
Joseph Wu
Thanks for Your answer.
So, it seems to be known issue with PGA280. My question will be now waht are the maximum rating for signal frequency and aplitude to avoid distortion. Can I find some recomendations in the data sheet? or waht can we do generally to avoid this distortion?
Thanks
Adrian
Adrian,
Currently, we don't have too much data on this phenomenon. However the development team is interested in who the customer is, what the application is and what the potential volumes are.
However, I would point out that since the distortion is above 20kHz, it is typically far above the usable frequency response of the digital filter in most of the oversampling converters in the product line.
Joseph Wu