This seems to be either not related or directly related to the INA282 causing a 15 amp bridge fuse to blow when B+ 169 DC is switched on.
To be clear 3 common mode shunts are monitored per page 24 figure 42 at the source of three FETS with individual 018 ohm current shunts very near ground potential on pin 1 & 8. The supply voltage of the INA282 is set at 2.975vdc providing an output center near 1.488 volts. The low/high side FETS gates are held low by three bridge drivers pre-powered from an isolated supply voltage before the B+ is switched on which then instantly blows the fuse.
Recently switched over from using 3 Opamps feeding into 3 separate ADC channels monitoring the three shunts which worked ok at 169 B+. The INA282 shunt monitors without blowing the fuse when (B+ is 20 VDC). Even after blowing the 15 amp fuse (B+169) several times the INA282 keeps on functioning as if nothing hazardous has occurred. After the fuse is replace and INA282 is tested once again to be functioning ok (B+20v).
Although the text states common mode limit of 80 volts, it is the posters belief the INA282 shunt input pin never should see anything close to 80 volts common mode being protected by each low side FET source, drain is 200BDV.
The INA282 data sheet page 24 states low side current monitoring has the added advantage of not be subject to any common mode transient artifacts.
1. Is switching on the 169 volts B+ such a transient to the INA282 and how can this blow the fuse?
2. Will adding a snubber diode (MUR300) cathode on pin1 or 8 to ground act as a transient suppressor without effecting the output signal or should a 75-78 volt zener be added?
Thanks for any ideas and or suggestions.