Other Parts Discussed in Thread: DRV103
I am working with a DRV103H (the 3A model with thermal pad) and noticing that it has output errors on 1.8A loads (6.5 ohm proportional solenoid).
I have uploaded two schematics one that works and one that does not.
There is an OK flag error in the middle of the voltage swing on the potentiometer however once the duty cycle is about 100% and the load is switched fully on the error light abruptly switches off and the solenoid runs normally until it overheats (about 15-20 sec) and turns off due to internal thermal protection circuitry.
Higher resistance loads (470 ohm) show completely normal operation on the oscilloscope.
To be clear I have a rudimentary setup for now with a simple 8 pin SOIC to DIP adapter plugged into a solderless bread board so it does NOT have adequate thermal protection for prolonged/continuous use. Hence the overheating but the device should function normally until it heats up and 15-20 seconds is plenty of time to swing through the range of available duty cycles especially when it is used on an extremely intermittent basis manually actuating the momentary switch on the enabler pin (8).
I suspect the capacitor may not be big enough (which I am going to try next) but is there anything obviously wrong?Schematics.pdf