We currently have 4-20mA sensors converting into a 0-5V analog signal from a shunt resistor. The signal is then fed into an isolated amplifier (ISO122) of which the output is connected to our COTS processing modules. We are now interfacing the analog signal to a TI microcontroller that is 3.3V IO tolerant. What is the best way of converting the 4-20mA signal into a 0-3.3V?
Can it still be done efficiency with the ISO122 or ISO124 but with a resistor divider? Would you suggest any other ways? An isolation barrier is required for us so please keep that in mind.
Thanks
-David