This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current Mirror 10nA to 10mA

Other Parts Discussed in Thread: LOG114

hi,

Does TI has any current mirror which is suitable for mirroring Photodetector currents from 10nA to 10mA?

Rgds,

kpk

  • Hi kpk,

    I do not find any TI product that is designed for that purpose. The REF200 has an internal mirror, but it isn't specified for such a very wide current range. 10 nA approaches the leakage current levels of bipolar transistors, and 10 mA is in the range where thermal effects can become an issue.

    Some LOG amplifiers can handle an input current range spanning 7, or 8 decades, but they are transimpedance amplifiers producing a voltage output, for a current input. The LOG114 is an example:

    www.ti.com/.../log114.pdf

    Regards, Thomas

    PA - Linear Applications Engineering