Other Parts Discussed in Thread: INA138
Hi,
i am using 100 khz as a switching frequency for buck regulator.
As per INA138 datasheet: Gain can be between 1 and 100 and output load resistance(or the gain) will affect the measurement bandwidth.
Moreover Electrical characteristic states that:
if RL = 5 Kohm , F = 800 khz
if RL = 125 Kohm, F =32 khz
Does it mean that for 100 khz switching frequency, maximum gain that can be selected is 8 and thus max output load resistance of INA138 is limited to 40 kohm ???
That means there is a direct relation of gain of the INA138 with the switching frequency of the buck regulator. Am i right or i am missing something???
Thank you in advance.