Other Parts Discussed in Thread: INA2128, INA128, INA2126, INA126
Hi,
I'm having a problem using the INA2128 with a load cell resistive bridge. circuit attached. The impedance of the bridge is approximately 1K. The exitation on the bridge is 8VDC. So the common mode voltage is about 4V. The bridge puts out a maximum differential voltage of 8mv. The supply for the INA2128 is 12VDC and GND. The reference voltage is 1.25VDC. I have a gain resistor of 40 ohms for a gain of 1251. A 10K resistive load on the output.
What i am seeing is the output limits to about 5-7volts? Looking at the data sheet I don't see why this should happen? I simulated it in TINA using your spice macro for the INA2128 and I see the same limitation. What is going on? Please HELP!