Other Parts Discussed in Thread: INA3221
E2e,
I am looking at the INA3221 and was wondering what the minimum voltage is that can be measured for the shunt voltage? I believe this is indicated by the LSB value for the shunt voltage, which is 40uV. So as I understand this, the INA will measure the shunt voltage in steps of 40uV. Therefore, the smallest value I can measure is also 40uV. I am trying to figure out what value of sense resistor I should use, and want to make sure that I do not pick a value that is too small to be registered at the minimum current.
For example, a value of 80mA and a .0005Ohm sense resistor would be the minimum possible current that I could measure (resulting in 40uV). Since it is a 13 bit ADC this results in 8192 steps (2^13), half of which are positive and half are negative (indicated in the -163.8mV to 163.8mV range).
Thanks for your help.
Regards,
WH