Other Parts Discussed in Thread: OPA2171
Hi,
Normally, in OPAMP datasheet, it is said that the device can operate across -45~85/125 in ambient temperature or free-air temperature.
1. Where the temperature is measured? How far between testing node and device?
2. What it the loading current when doing temperature performance evaluation? e.g. in OPA2171, the Rload = 10k Ohm across Ta = -40 to +125. Does it mean, the load resistor is 10K Ohm when the testing is performed across -40 to +125?
Thanks a lot.
Zhou