Part Number: OPA2197
I have used 2 opa2197(one chip) in differential amplifier configuration. One's output is connected to the other's input. My closed loop gain is(should be) ~3 for both of them. I have a signal of +-0.34V sinusoidal at the input of the first amplifier. Amplifiers' supply is +-9V. I want the input signal to be 400KHz. At low frequencies like below 50KHz everything seems to be normal. But as frequency goes up to ~280KHz the output gets larger (i.e. gain is increasing); after that frequency the output is getting smaller (i.e. gain is decreasing). What is the reason of this? What can I do?