Other Parts Discussed in Thread: OPA172, OPA316, INA826, INA118
differential receiver signal of anlog front end to single ended adc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
So to be clear, the ADC is in the Arduino, you just need the buffer in-between the sensor and the ADC; for that reason, I moved this thread to the Prec Amps Forum. Also, here is an ADC tool to use for the design of the front-end, Op Amp to ADC Circuit Topology Calculator: www.ti.com/tool/adc-input-calc . Voltage levels required would also be helpful.
~Leonard
Hello Mirza,
Could you provide the Ardruino model that you are using? This will help with understanding the ADC on board the Ardruino.
Best,
Errol Leon
Texas Instruments Inc.
Precision Op Amp Applications
Hello,
If the differential to single-ended circuit does not require very high input impedance, then a standard difference (or differential) op amp circuit will work fine. Consider using the OPA316 for <= +5V supplies and the OPA172 for >=4.5V supplies. Here's an example circuit using the OPA316 for a differential 0.5 - 4.5V input. .
If the circuit requires very high input impedance, consider a 3-op amp INA like the INA826.