Other Parts Discussed in Thread: INA148, INA149, INA111
Hello.
I need build a current sensor for a Full bridge inverter output.
The nominal output voltage of the inverter is 127 Vrms.
At their output there will gonna be a LC filter.
The main characteristic of the circuit is that the current is low, in the order of 100 mA, at most.
The basic schematic is below.
As I have some INA128 available, I intend to use it to sensing the output inverter current through Rshunt.
So there are three questions I need to ask:
1) This is a good ideia, use INA128 to measure such low current without using a high value of Rshunt?
2) In datasheet, there are Common-Mode Voltage Range ((V-) + 2 and (V+) - 1.4 V) and Safe Input Voltage (±40 V). Since the max power supply is ±18 V, could we put ±40 V at input?
3) My main concern is about input voltage regard to ground. Despite the maximum differential voltage on IN+ and IN- be low because the low current, the voltage at input pins regard to ground will be in the order of hundreds of volts. Can this IC withstand such a voltage level?
Thanks,
Henrique Luna (BR)