Part Number: OPA847
Other Parts Discussed in Thread: LMH6629
Hello
I buffered a small signal with a unity gain buffer in the front end of a sensor. the frequency range of the signal is 10KHz to 5MHz.
now I want to amplfy it with a gain +10V/V or +20V/V.
I'm surprised with two ultra-low noise IC such as LMH6629 and OPA847.
but the linearity has a key role in my application. (I have a 14Bit ADC)
at 1MHz: LMH6629 with a gain of +10V/V has a SFDR of 75dBc and with a gain of +20V/V has a SFDR of 71dBc.
as per OPA847 datasheet the OPA847 spice model can not predict well distortion:
http://www.ti.com/lit/ds/symlink/opa847.pdf page15
http://www.ti.com/lit/ug/tidu016/tidu016.pdf (a usefull document about OPA847)
But I think the linearity of OPA847 is better than LMH6629.
which one has better linearity?
Regards