Other Parts Discussed in Thread: INA330, OPA348
Hi,
The INA330 data sheet shows a PID example using a single op amp (figure 6), and also another example using separate P, I and D op amps (figure 7). The idea is to arrive at the R/C values using separate op amps, then using those values to arrive at the RC values of the single-op amp design.
How do you translate the RC values from the 3-op amp design to the single-op amp design?
Here is the same question phrased in more detail from my customer:
The datasheet for the INA330 Figure 6 shows an integrated PID controller based on the OPA348. Figure 7 shows another version of the PID with the Proportional, Integrator, and Derivative elements separated out into individual op amps. The paragraph above the figure states:
"The PID loop compensation can be optimized for loop stability and best response to thermal transients by adjusting C1, C2, C3, R2, R3, and R4... Figure 7 shows a circuit that can be used as an intermediate circuit to easily adjust components and determine system requirements."
Please provide the conversion equations to derive the C1, C2, C3, R2, R3, and R4 component values in Figure 6 PID, using the component values from empirically determined from the component values in the PID from Figure 7.
Thanks,
Rick