This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ua741cp voltage clamping

Other Parts Discussed in Thread: UA741, OPA251, OPA244, OPA241, OPA237, OPA211A, OPA211

I have a Ua741cp op amp and have noticed that it has a lower clamp of 2 volts and an upper clamp of -.5 volts from peak. I need to have a lower clamp of .5 volts or less. Is this chip defective? If it is not what model do I need to use to have a .5 volt lower clamp with the same package and pin configuration?

  • Hi Christian,

    The uA741 amplifier does not have a rail-to-rail output stage.  This means that the min/max voltage that the output stage of the amplifier can produce is smaller than the voltage on the supply rails. 

    A quick search using the Amplifier Selection Tool for rail-to-rail output stages with a max supply voltage up to +/- 15V yielded the following results:

    OPA251
    OPA244
    OPA241
    OPA237
    OPA234
    OPA211A
    OPA211

    Since there wasn't a lot of information I just guessed that the high-supply voltage was a requirement, if it is not, there are many other choices as well that may work for you and I would encourage you to try to search for the ideal amplifier for your application using the Selection Tool located in the "Amplifiers and Linear" section of the TI website.

    Best Regards,
    Collin Wells
    Linear Applications