Part Number: TL084M
Other Parts Discussed in Thread: LM139, LM311
I am evaluating a design submitted for evaluation by a vendor. I am responsible to review the design and give feedback about possible problems. The circuit uses a pair of TL084M op amps, one in a low pass filter application, which drives the 2nd op amp configured as a comparator (positive feedback). A snip of the circuit is shown, below: (Sorry for the low res. I can describe details needed.
The LPF is driven by the output of an LM139 comparator, with a pullup to +15 VDC via a 5.76 kOhm resistor. The LPF has a passband of about 9500 Hz. TL084M comparator has 100k feedback resistance and 20k source resistance.
I don't know this op amp, but would like to give some better feedback than "it is generally not a good idea to use a saturating op amp as a comparator, especially for slowly varying inputs". LM139 comparator is driven by a variable frequency, variable amplitude quasi-sine wave (fundamental with some unknown distortion) in the 100s Hz to 1000s Hz range. Comparator output drives a discrete BJT common-emitter inverter.
Any criticisms of this circuit or suggestions on specific problems it might see would be appreciated.