Part Number: THS4303
My setup:
Using THS4303EVM with a Rigol DSA-815 Spectrum analyzer and Tracking generator (TG) sweeping from 1Mhz to 1.5 Ghz. The THS4303EVM input is connected to the TG and the output is connected to the spectrum analyzer input. The power supply is +- 2.5V. The power supply current is 40 mA.
Does anyone have ( or can someone produce ) the expected output?
I expected the output amplitude to be flat beyond 1.5 GHZ.
I am seeing 100 to 300 mV with a 25mV input. This make no sense to me. I expect a gain of 2.5 V/V. Gain = .5 * 10 * .5, input 50 ohm "divider" X amplifier gain 10 X .5 output "divider" = 2.5.
Jim