Part Number: LMC6064
Other Parts Discussed in Thread: ADS7852, OPA4187
Hi guys,
My customer is using LMC6064 and has the following question:
I’m taking the reference of 2.5 from the ADS7852YB, doubling it to 5 using an OpAmp, then a second OpAmp unity gain as a buffer.
The problem that I’m having is the 2nd OpAmp is starting to oscillate. I’m using the LMC6064AIM.
At first I thought I had too much capacitance on the output, but I removed all the caps and it is worse.
This occurs with or without a load. The load is 8 RTD probes in parallel, one side to the 5 volt reference the other side to the 8 inputs to the ADS7852.
Each has a 3.01K resistor to ground. The 8 RTD probes are installed at MTA54.
This is probably something simple, but I just can’t see it.
Thanks,
Brian