Other Parts Discussed in Thread: LM311-N, LM211, LM111
I need to use the Strobe function, but not the Balance function. The note in Figure 12 says that if balancing is not used, then BALANCE and BAL/STRB pins should be shorted together. Yet Figure 13 only shows BAL/STRB being used during Strobing. Should the BALANCE and BAL/STRB pins be tied together when using the Strobe function and not the Balance function? What are the pros/cons of using BAL/STRB and leaving BALANCE open vs using BAL/STRB with BAL/STRB and BALNCE shorted together?