Part Number: PGA5807A
Dear E2E,
Do we have LNA solution which spec is shown in below?
Operating Frequency 734 ~ 960MHz
Gain 13 dB
NF 1.1 dB
Supply voltage 1.5~3.3V 2.8V (typ.)
BR,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.