Part Number: INA226
dear :
we use INA226 to measure about 15A to 20A current, what value Rshunt you suggest? what is the minimum value we can use ,is there any limitation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA226
dear :
we use INA226 to measure about 15A to 20A current, what value Rshunt you suggest? what is the minimum value we can use ,is there any limitation?
Hi,
You might want to check out this video that goes over how to choose the shunt resistor:
Regards, Guang
Hi,
Did you find the video helpful in answering your questions?
The system error versus your tolerance for the minimum detectable current determines the lowest shunt you can use.
Here is a rough hypothetical example – say the total error is 50uV referred to input and the minimum current you need to measure is 1A. And the maximum error you can tolerate is 10% at this current level. Then the shunt voltage would need to be at least 500uV. This voltage dictates the shunt resistance to be 0.5mOhm minimum. After selecting a shunt that satisfies this condition, check to see if the input is over range at the max current level. In this case 0.5*20=10mV, it is OK. Also compare this minimum value to your target max acceptable value.
You can adapt the above process to your specific current range and tolerance. In general it is better to choose a shunt as large as possible from pure measurement stand point of view.
Regards, Guang