Part Number: THS4031
Hello team,
Customer is working on a design with THS4031. They need to start sampling 2x the original speed at this point and it seems THS4031 will still be a good fit. How can we estimate how linear it is in the measuring range and how can we improve it?
Working conditions are:
- Dual Power supply = +/- 9VDC
- Gain between 1 and 3
- Output signal range is from 0 to 4Vdc (supports 16-bit ADC)
- Signal is the pulse (2MHz duration) and trying to measure amplitude of that pulse after signal is set up (99%).
Thank you!