Other Parts Discussed in Thread: TL074, TL082
Hello, In the SPEC of the Figure 6. Maximum Peak Output Voltage vs Load Resistance, it shows the VOM vs. RL.
However, the max. RL is 10K Ohm. What happens if the RL goes up to 100K Ohm? Very thanks.
Application: Industrial Motor
Regards
Brian Wang