Part Number: LM324
Other Parts Discussed in Thread: LM2902, , LM358, NE5532, SA5532
I am aware that these general purpose opamps (the LM324, LM358, LM2902, etc.) expect their load to be returned to ground, and provide a "Short-Circuit Output Current" specification in the datasheet. (Where "ground" may be a low-impedance node at a voltage between the supply rails, as in a split-supply application, or the low supply rail itself as in single-supply usage)
But many of them say shorting them to the high rail may cause overheating and destruction of the device.
So am I wrong to interpret that as meaning there is some maximum output current that we could cause to occur and must take care to avoid. And also that it is a maximum sink current, since the ability to short to the low supply rail surely means it's current-limited when sourcing current, right?
But there's nothing in the "Max" column under the row for "Output Current" on the datasheets!
| NE5532 / SA5532 |