Part Number: AMC1300
Other Parts Discussed in Thread: ISO120, ISO121, ISO224,
Hello,
I'm designing a high voltage(DC/AC) sensing circuit of signals that go up to 50kHz, However after doing simulation on TINA TI, it seems there starts to be a phase delay between the input and output signals after ~15kHz which corresponds to the datasheet. Is there an alternative option that I can use that is cheaper than the ISO120/ISO121 devices or additional components that would solve this issue?
Background: Designing circuit that can monitor input signals of up to ±1000V (DC and AC) up to 50kHz. The desired output will be ±10V which should be in phase with the input.
Thanks in Advance
Bright C