Part Number: INA148
Other Parts Discussed in Thread: PGA281
Dear Marek, thank you
I, probably, will use INA148 for receiving signal from a two-wire line. I have a long two-wire line - more than 10 km.
Please, report
1) What max DIFFERENTIAL input voltage can withstand INA148 ? Power supply is +/- 15 V.
I mean the maximum value of the voltage at which it will not fail.
2) I'd like to use circuit figure 5, page 10 of INA148 datasheet. How do you think, can I use it for receiving signal 50 - 1000 Hz, +/- 50 mV to +/- 12 V ?
3) Can you recommend amplifier with single-ended input and with digital control? Power supply +/- 15 V. Input signal frequency 50 - 1000 Hz, +/- 12 V . It is desirable that the minimum gain is 0.05 or close to that. I need single-ended amp with digital control to set after INA148.
TIA
Sincerely
Vladimir Naumenkov
www.agat.by