Hello,
I am Anirudh from GE Healthcare and want some information on Differential amplifier with following constraints:
1) High common mode voltage (Minimum of 100 volts)
2) Good differential Input voltage ( Around 20 volts)
3) Powered from single supply. (Ideally 5 volts)
4) Will be beneficial if it is a dual/quad op-amp.
Please recommend some IC numbers which can fulfill the above constraints. The priority of constraints is in the same manner as listed above.
Thanks