Other Parts Discussed in Thread: OPA189
Hi,
I'm trying to reconcile the OPA2189's capacitive drive (see typ op fig 26 which implies 1nF is close to the max capacitive load) with the differential gain applications figure (54) that shows a 1uF filtering cap being used with a differential gain configuration utilizing a 50-Ohm gain resistor. I'm pretty sure that this feedback resistor helps to isolates the amplifier from the capacitive load, is that right? Also, is there a way to understand the relationship between this resistance value vs. cap value and overshoot? Maybe a graph with curves for 0.1uF and 1uF cap values and different values of Rfb would be helpful.
Or, does this simulate well using TI's simulation tools?
Thanks!