Part Number: TL082
Hi All,
Can you help to analysis a TL082IDR failure?
The schmatic as following: The TL082IDR is used for highest voltage option circuit, these voltages represents different temperatures,these temperatures maybe same or not.Recently a TL082IDR is failure and as tested, find low resistance (132R) between non-inverting input (terminal 3) and negative power supply (terminal 4). Note: NO external FEA surge protection and EMI/RFI filiter part on schmatic.
I suspect:
The Amplifier looks like work as a voltage follower, but actual which is not work as a actual voltage follower. Since the inverting input is feedback the highest input voltage. Only one amplifier is work as a voltage follower, the rest amplifiers will work as comparator, as input voltage cannot keep Vin+=Vin-.
1. Any issue or concerns for following sch.
2. Any issue for TL082IDR in following application, wheather the TL082IDR can be used as a comparator or else issues or concerns?
3. Others reason caused amplifier failure. Pls correct if anythwhere is wrong or missing. Tks a lot.
BR,
Xiaobing (Eric)