Part Number: INA220
Other Parts Discussed in Thread: INA3221, INA231, INA230, INA233, INA226, INA260
Hi Team,
Customer is using the INA220 for monitoring the current across shunt in the battery application.
They are sampling the current every 2ms and computing the RMS over a time period of 10s. Customer see an abrupt value on one sample randomly, which is affecting the computation of the RMS and the subsequent averaging. What could be the possible reason for this abrupt value and any suggestion to mitigate it.
Any sample reference acquisition flow is recommended for the device?
The typical measured values are in the range of -0.32 to +0.32. The sudden abrupt reading is around 23.04.