This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which is the maximum operating temperature of the integrated shunt resistor?

Part Number: INA260


Hi TI team,

I designed a PCB where I use 2 INA260 in parallel to measure current up to 30A continuous and up to 40A with 60s current pulse. I'm using a thermal imaging camera to check the chip temperature at high current rate.

I see the shunt temperature to rise up to 125°C at 30A continuous and around 150°C at 40A after few seconds. The ADC part of the chip seems to remain in the operating range temperature.

I'm not sure if it is safe to use or if I have to change the PCB layout. In the datasheet is stated that the maximum junction temperature is 150°C.  Does it refer to the shunt part of the chip or it can reach higher temperature? 

  • Hi Ian,

    For over current conditions, please refer to datasheet section 8.3, specifically this figure:

    The max junction temperature refers to both the shunt and the chip, whichever is higher. At specified 15A, the shunt temperature is approximately 150°C. Your continuous condition test result is consistent with this specification (case temp 125°C).

    Regards, Guang