This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA855: Unity gain frequency of OPA855

Part Number: OPA855

Hello together,

I wanted to know unity gain frequency of OPA855. Is it equal to gain bandwidth product (GBWP) ?

Kind Regards

Selvedin Hodzic

  • The unity-gain bandwidth and GBW are similar, but the GBW is usually measured at a different frequency.

    A decompensated opamp like the OPA855 is not guaranteed to be stable at unity gain. As shown in figure 10, the unity-gain bandwidth would be at 8 GHz if the straight line would continue below 15 dB. But it does not, so it does not make sense to talk about what happens at 0 dB.