Hi folks,
I am looking for a cross or similar device to the Maxim MAX9632, which is discontinued. The equivalent could be in any package, but SOIC is preferred.
Please find some of the requirements below, is the OPA2182 a good alternative?
- It must be able to have supply range of at least +32V (for single supply), or +/- 16V (for dual supplies);
- It needs to have automotive temperature capability: -40C to +125C;
- It must have shutdown feature ( "SHDN" pin) , shown below;
Thanks,
AH