Other Parts Discussed in Thread: INA207
I am using the INA207 as a replacement of the MAX4375. Its larger input voltage range is an advantage and we started using the INA207 as a product replacement and for new designs. The exact part number I am using is INA207AIDGS.
If I apply 3.3V though a pull-up resistor to the CMP2 OUT pin with the remaining of the circuit unpowered, the open drain output is in an undefined state. In my circuit, the reset pin is connected to the ground
With a 10k resistor, the output is around 1.5V
With a 1k resistor, the output is around 2.0V
With a 100 ohm resistor, the output is around 2.2V
This unfortunate semi conductive open drain behavior is considered as an overcurrent detection in my circuit and the system cannot turns on.
I would like to know if there is a way to use the INA207 with a defined comparator output state at startup ?