Hello all,
I am looking for a high input impedance amplifier. The requirement is to amplify 10^-14 to 10^-13 amp current. Anybody can suggest which IC will work for it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I am looking for a high input impedance amplifier. The requirement is to amplify 10^-14 to 10^-13 amp current. Anybody can suggest which IC will work for it?
Hi Abhay,
Without knowing the type of application or requirements, here is a list of the ultra low Ibias or ultra high input impedance amplifiers. LMP7721 is one of the high input impedance op amp in the list of selections.

If you have additional questions, please let us know.
Best,
Raymond
Hello Kai,
Yes, it is a trans-impedance amplifier. Application is ion chamber current amplification.
Hi Abhay,
I know that these amplifiers are highly sophisticated. Can you show a schematic?
Kai