Hi, I need to detect the peak to peak amplitude of a sine wave with a frequency between 1.5 and 2.5 MHz. I do not want to use logarithmic amplifiers or RMS to DC converters since the change in my input is quite small (10 to 30% of initial) and those IC's give their outputs in a logarithmic scale. Hence, I would need a very high resolution ADC to detect the changes in the amplitude of the input. I thought of using a peak detector with a fast response op-amp. However I would need to discharge the output capacitor which holds the peak value and let it to be charged again with the new peak in order to detect the changes in the peak to peak amplitude of the input signal. I can add a triggering circuit, so the output capacitor would be periodically discharged and be ready for the new peak. But this would lead to glitches in the output that is going to be fed to the ADC and recharging of the capacitor will take some time and my lead to wrong (low) measurement. Any ideas? Best regards