Other Parts Discussed in Thread: INA333, OPA333, LM358
Hi everybody.
I have a problem using a INA333.
I'm using it for the measurement of a type J thermocouple for a project.
The temperature range my thermocouple will be on is between 0 and 100 °C, i'm gonna read the value on a microcontroller and do the cold junction compensation by the software method using another temp sensor which will be sensing the temp at the board or junction area.
my problem is that using the datasheet instructions for the right connections, i have no voltage (zero) at the Vout pin.
I used different gains, tested if my thermocouple is ok, used the special conectors for the type J thermocouple, and nothing happened.
I use a single voltage supply of 5v.
Could anyone please show me any circuit using what I mentioned before?......i think i'm missing something.
If you need additional info please let me know.