Other Parts Discussed in Thread: INA2128, INA333, INA128, INA111
Hello, I am getting the signal that you can see in the attached pdf5545.INA2128U noise.pdf from a bio-amplifier input stage made around one INA2128U. Bursts reach 120µVpp while the EEG machine used to see the signal has an input noise below 1µVpp in the band 0.08-90Hz 3dB. Both input positive and negative are bootstrapped through the INA2128 Rgain in/out pins, while the INA inputs are biased through a total 3.2Mohm. Input gain is 1X -no Rgain fitted-. It happens more or less the same with bias resistances tested up to 44Mohm (ground noise gets up, but not the 'bursts' or spikes shown). I have tested three different chips, soldered with hot air at a maximun temperature of 280Cº and all of them do the same. Any help?