This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Would you mind if we ask LM319 output voltage?
About following circuit, the value of output voltage is max4.28V. (It is 5-0.7V)
So, we guess that this voltage drop is caused by R12=13kΩ in the device.
Is our recognition correct?
So, it is not rail to rail type, right?
Kind regards,
Hirotaka Matsumoto
Hello Hirotaka,
The LM319 is an open-collector (O.C.) output. It *requires* an external pull-up for the output to go high. The output is not designed to source current.
Note that all the example schematics have a pull-up resistor, or a load tied to V+. Once you have proper value pull-up resistor, then the output will go to 5V. DO NOT rely on the internal leakages to pull the output high.
Also, the LM319 is not a rail-to-rail input device. The valid input range is +1 to +3V with a +5V supply (I am assuming V+=5V, V-=GND).
If the output is high, the input common mode range is violated (3.75V at +IN).
If your input sine wave is below 1V, or above 3V, it is in the "illegal" range, and the output can be in the wrong state when the input range is violated - possibly causing a "latch" condition with your circuit if a reversal occurs.
For your circuit above, with an input signal going 0-5V, you need a Rail to Rail input and output device like the LMV7239 or TLV3201 (assuming you need the ~100ns speed). Otherwise, there are numerous slower R-R I/O comparators to choose from.
Regards,
Paul san,
Thank you for your kindness and update!
We'd like to confirm one point.
About, input voltage range +1 to +3V with a +5V supply(V+=5V, V-=GND)
this value adapts to Input+ and Input-, doesn't it?
We need your help.
Kind regards,
Hirotaka Matsumoto
Hello Hirotaka,
The 5V spec line is for a "Single" supply, with V+=5V and V-=GND. The reference point is GND for single supply.
The spec applies to both inputs. Neither input should be less than 1V and greater than 3V.
The common mode voltage is NOT the average of the two inputs, as comparators can have several volts difference between the inputs. The spec is PER INPUT.
Regards,
Paul san,
Thank you for your input.
Ok, we got it!
Then we recommended to our TLV3201, 3202 and LMV3279 if our customer needs rail to rail input type.
Kind regards,
Hirotaka Matsumoto