Part Number: AMC1100
Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301,
Hello,
I am using DRV8301 kit along with Picolo F28069M.
Kindly refer page 6 of the following document.
BOOSTXL-DRV8301 Hardware User's Guide (SLVU974–October 2013)
At present i am making a motor controller which has an isolated voltage sense requirement.
I want to make an isolated voltage sensor to sense the Dc bus as well as motor phases using AMC1100
which has a voltage filter pole of 364.692 Hz
Kindly help
Thanks and regards.