Dear sir,
we have testes the above LM2907-M of frequency to voltage converter with a input from frequency analyzer with an input of square wave of duty cycle 50% and a VCC of 5v with is we got an output which is varing with the frequency with an 0.0011 volts per one HZ i.e 891 Hz per one volt with an R1=100k and C1=22nf.
so we test with an practical circuit of your unit which is an BLDC motor with a hall frequency of 650HZ and other frequency signal of 3.81khz but we getting the output Vout=0v, which is not varing with the frequency signal which is a duty ratio of pulse waveform of 50% duty cycle.
can you please answer the above question why it is not varing the input hall Frequency of motor and can you share the schematic values which is suitable for the test.