Other Parts Discussed in Thread: AFE5801, AFE5801EVM
I recently purchased the AFE5801 EVM and TSW1400. Right now I am just trying to verify that the signals go through and are captured by TSW1400. Somehoe i cannot things to work. A few details on my setup:
1. I am using the AFE in internal 40MHz CLK mode. My understanding is that the default position of P4 jumper would suffice, so I am not doing anything to supply the external clock.
2. For some reason, the tab on AFE GUI (TI ADC SPI interface) shows "Init for TSW 1250" instead of TSW 1400. Is that okay?
3. Input to channel 8 of ADC is 2 MHz Sin wave as described in the user manual. When I select FFT mode on HSDC Pro (TSW's GUI), I can only see noise floor, even time domain data doesn't make any sense. In fact even if i remove the input signal, i can just see noise floor. Somehow it seems that signal is not passing through AFE. AFE gain is set to 30dB, i tried to change it but no help.
I think I am missing something basic. Please advise.
-Gaurav