Other Parts Discussed in Thread: LP8731-Q1, LP8732-Q1
Hello Champs,
As you may aware of this TIDesign, TIDA00530 (
), it specified usability of LP8731.
So one of my customer would like to use 1~2ea of LP8731-Q1 or LP8732-Q1 as TDA3x power source(PMIC).
But one concerning point is their initial value for two DCDCs and two LDOs.
The initial values are : 1.0625V(Buck1), 1.0625V(Buck2), 2.8V(LDO1), 3.3V(LDO2).
And the this TIDesign user manual said, it should need to be reprogrammed after power-up of TDA3x, or factory OTP setting can be possible(but it will required in customer application which has over certain volume).
In the TDA3x datasheet, it should be 1.15V(nominal) at the BOOT condition for both CORE and DSPEVE.
So could you please check and confirm LP873x-Q1 can be used for the TDA3x application, while doing reprogram at the booting sequence?
Regards,
Ernest Cho