Hi,
I am trying to use the Usecase generation tool to create the .jpg file in radar SDK. I am using the following command to create these files(usecase_name.priv.c , usecase_name.priv.h, usecase_name.jpg files)
Command is: vsdk_win32.exe PATH_TO_USECASE_FOLDER/usecase.txt -img -file -path PATH_TO_USECASE_FOLDER/
I was able to create all the files successfully in Vision-SDK, But here I came across with an error saying about the compatibility issue since my system is of 64 bit. (Didnt come across this error while in Vision-SDK )
When I use vsdk_win64.exe trying with the same command, jpeg file is not created and the rest of the files are being created. And when I use executable "vsdk_win32.exe" present in visionSDK 3.2 and provide the usecase of RADAR-SDK , the jpeg is being created.
Command is:
vsdk_win32.exe PATH_TO_USECASE_FOLDER_IN_RADAR-SDK/usecase.txt -img -file -path PATH_TO_USECASE_FOLDER_IN_RADAR-SDK
In all the cases I have set the PATH to the Graphviz tool. I do not understand what is the issue with the RADAR-SDK's vsdk_win32 .exe
Thanks & Regards,
Varsha