Other Parts Discussed in Thread: AM3352
Hi,
We are working on the AM335X RTC. We can use the AM335X internal32.768KHz clock source to clock RTC, but when the system is powered off, we find the internal clock souce doesn't drive the RTC.
So we try to use the external 32,768 cyrstall as the source to the AM335X RTC click input, But the crystal cannot oscillate and RTC cannot start.
The following is RTC registers value. And the RTC external cyrstal circuit is attached too,
Please help to see if anything wrong in our design or the regisers setting.
Thanks,
Peng
44e3e000: 00000000 00000000 00000000 00000001
44e3e010: 00000001 00000000 00000000 00000000
44e3e020: 00000000 00000000 00000002 00000002
44e3e030: 00000004 00000000 00000000 00000000
44e3e040: 00000001 00000000 00000008 00000000
44e3e050: 00000000 00000008 00000000 00000000
44e3e060: 00000000 00000000 00000000 00000000
44e3e070: 00000000 4eb01106 00000002 00000000
44e3e080: 00000000 00000000 00000000 00000001
44e3e090: 00000001 00000000 00000000 00000000
44e3e0a0: 00000000 00000000 00000000 00000000
44e3e0b0: 00000000 00000000 00000000 00000000
44e3e0c0: 00000000 00000000 00000000 00000000
44e3e0d0: 00000000 00000000 00000000 00000000
44e3e0e0: 00000000 00000000 00000000 00000000
44e3e0f0: 00000000 00000000 00000000 00000000