This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: DDR issue

Part Number: AM3352


The 1st spin of our custom board (based on the BeagleBone Black) used the AM3352 with a single Micron MT41K256M16HA-125 and we've already successfully ported U-Boot/SPL and Linux to that.

The 2nd spin is using the a single Micron MT41K256M16TW-107 as a BoM modification, layout has not been changed.

I've been trying to discover the DDR timings for the 2nd spin and unfortunately I'm seeing the "Data Changing Everywhere!" symptom as described here.

I'm attempting to configure the RAM to 6-6-6 800MT/s @ 400MHz. Using the datasheet for MT41K256M16 I came up with the values below:

Memory datasheet symbol Memory Datasheet value unit
tCK 2.5 ns
tRP 15 ns
tRCD 15 ns
tWR 15 ns
tRAS  37.5 ns
tRC 52.5 ns
tRRD 10 ns
tWTR 10 ns
tXP 3 tCK
tAOND 2 tCK
tXSNR 170 ns
tXSRD 512 tCK
tRTP 10 ns
tCKE 3 tCK
tRFC 160 ns

and from the CAD:

Parameters
DDR clock frequency 400 MHz
PHY_INVERT_CLKOUT 1
Trace Length (inches)
Byte 0 Byte 1
DDR_CK trace 0.823 0.823
DDR_DQSx trace 1.064 0.969
Intermediate values (per byte lane)
WR DQS 7B 7D
RD DQS 40 40
RD DQS GATE F6 F2
Seed values used in CCS code
DATAx_PHY_RD DQS_SLAVE_RATIO 40
DATAx_PHY_FIFO_WE_SLAVE_RATIO F4
DATAx_PHY_WR DQS_SLAVE_RATIO 7C
Register value
CMDx_PHY_CTRL_SLAVE_RATIO 100

GEL file:

//******************************************************************
//EMIF parameters
//******************************************************************
// DDR3 400MHz settings -- Needs modified

#define ALLOPP_DDR3_READ_LATENCY    0x07        //RD_Latency = (CL + 2) - 1

//400MHz settings for 4Gb device -- Needs modified
#define ALLOPP_DDR3_SDRAM_TIMING1   0x0AAAE51B
#define ALLOPP_DDR3_SDRAM_TIMING2   0x24437FDA
#define ALLOPP_DDR3_SDRAM_TIMING3   0x000003FF

#define ALLOPP_DDR3_SDRAM_CONFIG    0x61C05332  //termination = 1 (RZQ/4)
                                                //dynamic ODT = 2 (RZQ/2)
                                                //SDRAM drive = 0 (RZQ/6)
                                                //CWL = 0 (CAS write latency = 5)
                                                //CL = 4 (CAS latency = 6)
                                                //ROWSIZE = 6 (15 row bits)
                                                //PAGESIZE = 2 (10 column bits)
#define ALLOPP_DDR3_REF_CTRL        0x00000C30  //400 * 7.8us = 0xC30
#define ALLOPP_DDR3_ZQ_CONFIG       0x50074BE4

Summary:

  1. Software levelling always fails with all zeros
  2. "Data changing everywhere!" When looking at 0x80000000 with continual refresh

Please advise.

EDIT: Attached datasheet.4Gb_DDR3L.pdf

  • This is practically the same memory. Have you tried with your old settings?
  • Yes, the original settings were the first that I tried. They did not work for our rev B.
  • Hi Stephen,

    I was wrong in my question!

  • Hi Stephen,

    I found the refreshing timing parameters to be different from what is expected in the datasheet

    For a 4Gb, trfc is 104 CK = 260ns. But you have taken as 160ns. Also the corresponding tXSNR, should be 270ns
  • What Dwarakesh has noticed is correct. Please double check your timings. The timing register settings should be the only difference.
  • Thank you both. With those changes the data changing appears to be less random, however I'm still seeing "all zeros" and "data changing everywhere".

    I've attached a 5 second animated GIF to show what I'm seeing.

    Is there somethings else that's just slightly off?

  • Please post your timing spreadsheet.
  • Can you try with these timings: (Use table in my post below)

  • Thank you, I have tried those timings.

    Please see attached GIF for behaviour after running the slave ratio search program. It seems to be similar to before?

  • Hi Stephen,

    One observation in the AM335x_DDR_register_calc_tool - micron.xls, you are using the sheet for DDR2, instead of DD3 sheet. I am not sure what could be the difference. But you can give a try by entering in the proper DDR3 sheet and check.
  • Oh, my... Thanks for noticing this Dwarakesh!
  • Unfortunately I still see the same problem.

    Thank you for pointing that out though, Dwarakesh - I didn't even notice the other sheets!

    The ALLOPP_DDR3_SDRAM_TIMING are now almost identical to Rev A, in fact they actually work on the Rev A board but I have to use different _PHY_ constants:

    # This works for Rev A...
    #define  CMD_PHY_CTRL_SLAVE_RATIO       0x80
    #define  CMD_PHY_INVERT_CLKOUT          0x0
    
    #define  DATA_PHY_RD_DQS_SLAVE_RATIO    0x39
    #define  DATA_PHY_FIFO_WE_SLAVE_RATIO   0x97 //RD DQS GATE
    #define  DATA_PHY_WR_DQS_SLAVE_RATIO    0x41
    #define  DATA_PHY_WR_DATA_SLAVE_RATIO   0x7B  //WRITE DATA
    
    #define ALLOPP_DDR3_READ_LATENCY    0x07        //RD_Latency = (CL + 2) - 1
    
    #define ALLOPP_DDR3_SDRAM_TIMING1   0x0AAAD4DB
    #define ALLOPP_DDR3_SDRAM_TIMING2   0x266B7FDA
    #define ALLOPP_DDR3_SDRAM_TIMING3   0x501F867F
    
    #define ALLOPP_DDR3_SDRAM_CONFIG    0x61C05332
    

    I can't seem to get the slave ratio program to return anything but zeros for Rev B, even if I try the Rev A seed values. In fact if I do that then the memory browser just shows all zeros as well.

    So using what we've discussed...

    # This is what I have so far for Rev B...
    #define  CMD_PHY_CTRL_SLAVE_RATIO       0x100
    #define  CMD_PHY_INVERT_CLKOUT          0x1
    
    #define  DATA_PHY_RD_DQS_SLAVE_RATIO    0x40
    #define  DATA_PHY_FIFO_WE_SLAVE_RATIO   0xF4 //RD DQS GATE
    #define  DATA_PHY_WR_DQS_SLAVE_RATIO    0x7C
    #define  DATA_PHY_WR_DATA_SLAVE_RATIO   0x80  //WRITE DATA
    
    #define ALLOPP_DDR3_READ_LATENCY    0x07        //RD_Latency = (CL + 2) - 1
    
    #define ALLOPP_DDR3_SDRAM_TIMING1   0x0AAAD4DB
    #define ALLOPP_DDR3_SDRAM_TIMING2   0x266B7FDA
    #define ALLOPP_DDR3_SDRAM_TIMING3   0x501F843F
    
    #define ALLOPP_DDR3_SDRAM_CONFIG    0x61C05332
    

    With the above I still see the same "data changing" in memory browser...

    One thing that I think is strange is that the seed values from the RatioSeed spreadsheet don't work and aren't used for Rev A, I would've thought they'd be the same between the two boards if layout hadn't changed? When I originally did the bringup for Rev A I just used the BeagleBone Black seed values from the tutorial and they worked.

    Now when I'm trying Rev B, I've tried both the seed values from Rev A and also the ones provided by the RatioSeed spreadsheet. If I use Rev A seeds values I see all zeros in the memory browser, if I use the RatioSeed spreadsheet values then I see the data changing as per the GIFs previously posted.

    I'm at a loss now. Could this be an issue with impedance matching on Rev B? Or am I missing something?

  • Hi,

    We all did that mistake. I was referring to the wrong sheet yesterday :) . Biser is the right person to answer, since he is an expert in hardware, but from what I have very limited knowledge, the Seed Ratio spread sheet should be filled with the trace length in your actual layout. If the layout has changed between revA and revB, you might need to provide the correct changed values and by trying out various other Boards' may not help.

  • I've had confirmation that the layout has not changed so the trace lengths are the same for rev A and B.
    So in theory the slave ratio values should be the same.
    I know the timing register values that Biser suggested work on rev A with the rev A slave ratios.
    Which in turn would suggest that the same GEL file should work for both revisions and that the original timings should in fact work for rev B as well.
    So logically I'm being led to believe this may be a hardware issue of some sort?
  • Stephen, a lot of times when the software leveling algorithm returns zeros, it is because the processor is not in supervisor mode.  I have seen this quite often with CCS, especially ver 6.x and later.  CCS will put the processor in user mode when loading a program.

    After loading the file, ensure that the processor is in supervisor mode before executing the software leveling algorithm by executing the script Script->default->AM335xStartState.  You can check the processor mode in the bottom right corner of the CCS Window as shown below

    Regards,

    James

  • Hi James, thank you for the suggestion however it appears that supervisor mode is activated correctly without the need to run a script.

    I've uploaded a complete screencast of the CCS session below (5MB animated GIF) in case you spot anything else? In the screencast I use the seed values from the SeedRatio spreadsheet, although I see the same behaviour if I use the seed values from rev A. I also see the same behaviour if I use the timing registers from rev A or, as in the screencast, the timing registers provided by Biser. I've also tried all combinations of the above to the same effect.

    When I follow the exact same process for a rev A board, the levelling works correctly (with rev A seed values entered into GEL file and console) either with the rev A timing registers or with the timing registers provided by Biser.

  • Stephen, can you try increasing your READ_LATENCY by 1.  If it still doesn't work, try by 2

    Regards,

    James

  • Hi, thanks for your help so far. I just thought I'd add something that may or may not be relevant. the Clock speed in the details Stpehen sent over is DDR clock frequency 400 but the memory speed is 800 mghz. Could this be the issue? the data is being moved too quickly?

    Many Thanks

    Paul...
  • Paul, that shouldn't be an issue.  We support a DDR clock frequency of 400MHz (ie, 800M T/s).  The minimum speed grade that we support for 400MHz operation is DDR-1600, which both of your devices meet.

    Any results of the read_latency tests?

    Regards,

    James

  • Thanks all for help and clarification. An issue was found with our layout regarding DDR_VREF.