Other Parts Discussed in Thread: AM4376, DP83848C, TPS65218
Hi,
I have a am4376 based custom board with dp83849ivs [instead of KSZ9031RN in EVM].
I made below changes in code but still unable to send or receive data through eth0.
Could you please check the below changes and guide us to resolve the issue.
Disabled the MAC in u-boot Device tree:
-&mac {
+/* &mac {
slaves = <1>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
-};
+}; */
Added the mux entries in u-boot mux.c
+
+static struct module_pin_mux mii1_pin_mux[] = {
+ {OFFSET(mii1_txen), MODE(0)},
+ {OFFSET(mii1_rxdv), MODE(0) | RXACTIVE},
+ {OFFSET(mii1_txd3), MODE(0)},
+ {OFFSET(mii1_txd2), MODE(0)},
+ {OFFSET(mii1_txd1), MODE(0)},
+ {OFFSET(mii1_txd0), MODE(0)},
+ {OFFSET(mii1_txclk), MODE(0)},
+ {OFFSET(mii1_rxclk), MODE(0) | RXACTIVE},
+ {OFFSET(mii1_rxd3), MODE(0) | RXACTIVE},
+ {OFFSET(mii1_rxd2), MODE(0) | RXACTIVE},
+ {OFFSET(mii1_rxd1), MODE(0) | RXACTIVE},
+ {OFFSET(mii1_rxd0), MODE(0) | RXACTIVE},
+ {-1},
+};
+
+static struct module_pin_mux mii2_pin_mux[] = {
+ {OFFSET(gpmc_a0), MODE(1)},
+ {OFFSET(gpmc_a1), MODE(1) | RXACTIVE},
+ {OFFSET(gpmc_a2), MODE(1)},
+ {OFFSET(gpmc_a3), MODE(1)},
+ {OFFSET(gpmc_a4), MODE(1)},
+ {OFFSET(gpmc_a5), MODE(1)},
+ {OFFSET(gpmc_a6), MODE(1)},
+ {OFFSET(gpmc_a7), MODE(1) | RXACTIVE},
+ {OFFSET(gpmc_a8), MODE(1) | RXACTIVE},
+ {OFFSET(gpmc_a9), MODE(1) | RXACTIVE},
+ {OFFSET(gpmc_a10), MODE(1) | RXACTIVE},
+ {OFFSET(gpmc_a11), MODE(1) | RXACTIVE},
+ {-1},
+};
@@ -134,6 +167,8 @@ void enable_board_pin_mux(void)
configure_module_pin_mux(mmc0_pin_mux);
configure_module_pin_mux(i2c0_pin_mux);
configure_module_pin_mux(mdio_pin_mux);
+ configure_module_pin_mux(mii1_pin_mux);
+ configure_module_pin_mux(mii2_pin_mux);
Below changes in Linux device tree:
=============================
diff --git a/arch/arm/boot/dts/am437x-gp-evm.dts b/arch/arm/boot/dts/am437x-gp-evm.dts
index 49ab9520f16..083ede3d3e0 100644
--- a/arch/arm/boot/dts/am437x-gp-evm.dts
+++ b/arch/arm/boot/dts/am437x-gp-evm.dts
@@ -246,44 +246,50 @@
>;
};
+ cpsw_default: cpsw_default {
+ pinctrl-single,pins = <
+
+ /* Slave 1*/
+ /* 0x108 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) */ /* (D16) mii1_col.gmii1_col */
+ /* 0x10c ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) */ /* (B14) mii1_crs.gmii1_crs */
+
+ 0x110 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (B13) mii1_rx_er.gmii1_rxer */
+ 0x114 ( PIN_OUTPUT_PULLDOWN| MUX_MODE0) /* (A13) mii1_tx_en.gmii1_txen */
+ 0x118 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (A15) mii1_rx_dv.gmii1_rxdv */
+ 0x12c ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (D14) mii1_tx_clk.gmii1_txclk */
+ 0x130 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (D13) mii1_rx_clk.gmii1_rxclk */
+ 0x128 ( PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* (B15) mii1_txd0.gmii1_txd0 */
+ 0x124 ( PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* (A14) mii1_txd1.gmii1_txd1 */
+ 0x120 ( PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* (C13) mii1_txd2.gmii1_txd2 */
+ 0x11c ( PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* (C16) mii1_txd3.gmii1_txd3 */
+ 0x140 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (F17) mii1_rxd0.gmii1_rxd0 */
+ 0x13c ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (B16) mii1_rxd1.gmii1_rxd1 */
+ 0x138 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (E16) mii1_rxd2.gmii1_rxd2 */
+ 0x134 ( PIN_INPUT_PULLDOWN | MUX_MODE0 ) /* (C14) mii1 */
+
+
+ /* Slave 2 */
+ /* 0x78 ( PIN_INPUT_PULLUP | MUX_MODE1 ) */ /* (A3) gpmc_be1n.gmii2_col */
+ /* 0x84 ( PIN_INPUT_PULLUP | MUX_MODE8 ) */ /* (F10) gpmc_csn2.gmii2_crs */
+
+ 0x74 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (B3) gpmc_wpn.gmii2_rxer */
+ 0x40 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* (C3) gpmc_a0.gmii2_txen */
+ 0x44 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (C5) gpmc_a1.gmii2_rxdv */
+ 0x58 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (E8) gpmc_a6.gmii2_txclk */
+ 0x5c ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (F6) gpmc_a7.gmii2_rxclk */
+ 0x54 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* (E7) gpmc_a5.gmii2_txd0 */
+ 0x50 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* (D7) gpmc_a4.gmii2_txd1 */
+ 0x4c ( PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* (A4) gpmc_a3.gmii2_txd2 */
+ 0x48 ( PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* (C6) gpmc_a2.gmii2_txd3 */
+ 0x6c ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (D8) gpmc_a11.gmii2_rxd0 */
+ 0x68 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (G8) gpmc_a10.gmii2_rxd1 */
+ 0x64 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (B4) gpmc_a9.gmii2_rxd2 */
+ 0x60 ( PIN_INPUT_PULLDOWN | MUX_MODE1 ) /* (F7) gpmc_a8.gmii2_rxd3 */
- cpsw_default: cpsw_default {
- pinctrl-single,pins = <
- /* Slave 1 */
- 0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_txen */
- 0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rxctl */
- 0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_txd3 */
- 0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_txd2 */
- 0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_txd1 */
- 0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_txd0 */
- 0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rmii1_tclk */
- 0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rmii1_rclk */
- 0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rxd3 */
- 0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rxd2 */
- 0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rxd1 */
- 0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rxd0 */
- >;
- };
+ >;
+ };
- cpsw_sleep: cpsw_sleep {
- pinctrl-single,pins = <
- /* Slave 1 reset value */
- 0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
- 0x134 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
- 0x138 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
- 0x13c (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
- 0x140 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
-
- >;
- };
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
@@ -1034,9 +1040,10 @@
&mac {
slaves = <1>;
- pinctrl-names = "default", "sleep";
+ /* pinctrl-names = "default", "sleep"; */
+ pinctrl-names = "default";
pinctrl-0 = <&cpsw_default>;
- pinctrl-1 = <&cpsw_sleep>;
+/* pinctrl-1 = <&cpsw_sleep>; */
status = "okay";
};
@@ -1048,8 +1055,8 @@
};
&cpsw_emac0 {
- phy_id = <&davinci_mdio>, <0>;
- phy-mode = "rgmii";
+ phy_id = <&davinci_mdio>, <3>;
+ phy-mode = "mii";
};
minicom log :
eth0 Link encap:Ethernet HWaddr C4:BE:84:CB:12:32
inet6 addr: fe80::c6be:84ff:fecb:1232%132688/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:43 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:7637 (7.4 KiB)
Interrupt:143
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%132688/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:323 errors:0 dropped:0 overruns:0 frame:0
TX packets:323 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:24632 (24.0 KiB) TX bytes:24632 (24.0 KiB)
root@am437x-evm:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Link partner advertised pause frame use: Symmetric Receive-only
Link partner advertised auto-negotiation: Yes
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 3
Transceiver: external
Auto-negotiation: on
Supports Wake-on: d
Wake-on: d
Current message level: 0x00000000 (0)
Link detected: yes
I attached pin compare diagram
Thanks in advance